AXIS#.SAFE.FSOE.APPLPARAMLENGTH

Description

Indicates the size of the FSoE application parameters. If using WorkBench safety parameters, this is 0 and if using application parameters over FSoE it is 4 bytes.

Context

For complete FSoE information refer to the AKD2G EtherCAT Manual.

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read Only

Units

N/A

Range

0-65535
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
AXIS1.SAFE.FSOE.APPLPARAMLENGTH

e901h

08h

Unsigned16

-

-

Read only

No

AXIS2.SAFE.FSOE.APPLPARAMLENGTH

e911h

08h

Unsigned16

-

-

Read only

No